Part Number: TXB0104
Other Parts Discussed in Thread: TMS320F28034, SN74AVC4T774, SN74LVC2T45, SN74LV4T125, SN74LV1T126, SN74LVC1T45
Good morning, i am using TXB0104 for shifting SPI signal of 3.3V from a DSP (in particular TMS320F28034) to 5V SPI for interfacing with a slave SPI device.
I read of possible problem of TXB0104 to drive some loads in its I/O pin in DC. For example, CS signal remains low for enough time during the transition: it is a problem for the TXB0104 to mantain this DC low level? How much is its load current and capacitance capability? Another example could be when MISO or MOSI (for example in a 8 bit SPI communication) have all bits to 0 or all bits to 1 for the entire time. Could this example be another problem for the peripheral?
Is it necessary to use a buffer?
Thank you.