Part Number: TXB0102
Other Parts Discussed in Thread: TXS0102
Would like to use the TXB0102 to translate a 5V ultrasonic sensor to 1.8V GPIO. Concern about possible timing delay. Is there a timing spec define rated across temp.. Particularly interested in the -40C and 85C temp ranges. Since delays in timing the can effect the distance measured by the ultrasonic sensor. Also is there a recommended voltage translator that can be used for both I2C and GPIO interfaces.
I2C is open drain and GPIO needs both High and Low level for translation. Would like a single IC if possible to have both capabilities.
Thanks,
Tenyu