This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV4T125: SPI repeater

Part Number: SN74LV4T125
Other Parts Discussed in Thread: SN74LVC125A, SN74AHC367

Dear all,

 We have application using SPI communication with 40cm long distance form CPU to other devices, need add SPI repeater to guarantee the normal communication, can SN74LV4125 used in this application? the communication rate is 50MHz, and the input voltage is 3.3V and Vcc also should be 3.3V.

Thanks.