How are setup and hold time margins calculated?
I design Analog mostly, but now I have my hands on digital systems. I was not able to find a good description on google.
Any books or app notes?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Setup and hold times are not calculated they are actually measured. The area between the setup and the hold times is where you would not want the clock to change if you expect the output to be effected. Here is an appnote with some explaination.
There are no setup an hold time skews. They are tested so that if you stay within the limits the part should work correctly across temp and process. Although there may be some skew on actual setup and hold times, you should not have any signal changing in this area if you go by the datasheet limits.
Are there several methods to measure setup and hold time?
For example: to measure input setup and hold with respect to clock, do we move data rising edge independent of data falling edge.
Is the setup time measured by moving the window or only the edge from left to right?
Similarly measure hold time from moving the second data edge from right to left while keeping edge one fixed?
Setup and hold time are measured by moving the edge of the data in reference to the clock until you see a fail.