Other Parts Discussed in Thread: SN74LVC2G07
Hi ,
I am looking for a level translator with the following requirements:
Inputs :5V TTL and 5V CMOS
Output: 3.3V CMOS
Bidirectional type
2 Channels per port
It would be great if i can get a two devices with Pin to Pin compatible (for easily replacing the IC if i use 5V TTL peripheral or 5V CMOS peripheral)
Is it possible to get an device like this ?
Looking for your reply at the earliest
Regards,
Rajesh