This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TWL1200-Q1: Interface compatible with AM4376 and WL1837MOD

Part Number: TWL1200-Q1


Hi,

We are looking to interface the WL1837MOD which has 1.8V SDIO lines to our 3.3V IO lines on the AM4376. Looking on page 4 of this report for level shifting the WL1837MOD IOs: http://www.ti.com/lit/an/swra448a/swra448a.pdf, I see that we have an example of doing this using the TXS0108E device. What is the difference between this device and the TWL1200-Q1


On TWL1200-Q1 datasheet mentioned about the 1.8V and 3.3V IO line interface 

Please also feel free to recommend any devices that might work in this case.