Other Parts Discussed in Thread: TXS0108E, TXS0206, TXS0206A
Hi, now I am using TXB0108 between i.mx6-CPU and SD card interface for my prototype.
VCCB side is used for CPU (3.3V), VCCA side is used for SD card (battery backuped by approximately 3.4V)
In SD card specifications, class10 is enough for me.
I have two questions.
1.
Contrary to TXB0108 datsheet, VCCA is a little higher than VCCB by 0.1V.
But according to the application report below,
if the voltage difference is under 0.6V, it seems that any problems won't occur.
Is it OK for my how to use?
2.
Though TXB's drive strenght is too low, now my prototype began to run in some way.
I am worried whether I should keep to use TXB0108 for mass production.
But in the other device such as TXS0108E or TXS0206,
TXS0108E's internal pull up resisters are invalid when OE is low level and then TXS0206 is hard to mount for us due to its 0.4mm pitch BGA package.
Is it OK to use TXB series for class10 SD card interface?