Part Number: LSF0108-Q1
Hi team,
I have a question for swithc pass voltage.
I am looking at the following expression in the datasheet.
"Rpu = (Vpu – 0.35 V) / 0.015 A"
I understand that this formula limits the pass voltage to 0.35 V or less at 15mA, but can you think that it is satisfied at all temperature conditions?
In other words, is there no doubt that Ron of the switch does not exceed 0.35 V / 0.015 A = 23.3ohms under all temperature conditions?
In the data sheet ron is mentioned only typical, I do not know whether it can guarantee 350 mV or less even in the worst condition.
We are considering two patterns when Vref_A is 1.8 V and Vref_B is 3.3 V, Vref_A is 1.8 V and Vref_B is 5 V.
We must do it drop in the switch must be 350 mV or less even in the worst case.
Best regards,
Tomoaki Yoshida