Part Number: TXB0106
Hi, I am confused about the statement below.
Which is right 1 or 2 ?
Thank you in advance,
yukihiro.
1.
community title : TXB0106: TXB0106 for SD-card???
The TXB0106 is primarily designed for push/pull signals; SD cards use open-collector signals. And it's likely that the TXB's drive strength is too low.
2.
community title : NEW FAQs
TXB (www.ti.com/.../SCEA043)
The TXB push-pull buffered type architecture does not require a DIR control signal to establish the direction of data flow.
This architecture is designed to exclusively be connected and interfaced with a push-pull CMOS driver and is capable of driving a capacitive or high impedance loads in applications such as Secure Digital (SD) or Serial Peripheral Interface (SPI).
The TXB010x devices are not intended for use in open-drain applications.