For board to board communication, We used Level translator driver IC's. Board 1 have FPGA, the output line 3.3V is connected to SN74ALVC164245DGGR (+3.3V to +5V ) Level translator. Output (+5V) of the level translator is connected to Connector (PMC). My requirement is, the +5V output to be connected into two SN74LVC4245APWR device (Board 2 and Board 3).
I seen in SN74ALVC164245DGGR datasheet, Ouptut clamp current is -50mA in Maximum Absolute rating. In-case after connecting two SN74LVC4245APWR device, the sing current will be around ~48mA.
I want to know, any possible is there to operate the single SN74ALVC164245DGGR into two SN74LVC4245APWR device.