Part Number: SN74LVC2G07
Other Parts Discussed in Thread: STRIKE
Hi,
We currently encounter a strange situation (unexpected voltage level) at pin1 (1A) of SN74LVC2G07. As shown below, USB_0_1_OC_N is from another chip with open drain output in the original design, so customer implement external pull-up resistor (R1261) to P3V3_STBY. For testing purpose, now customer disconnect USB_0_1_OC_N trace on the board so that SN74LVC2G07 pin1 is only connected to the 33ohm (R1187) and then 10kohn(R1261) to P3V3_STBY.
For such connection, we expect pin1 to be 3.3V, but found it's only 2.8V. If we do the same thing at pin3 (2A), the voltage is 3.3V as expected. Meanwhile, the output voltage lvel at 1Y and 2Y are normal. Can you explain why we see 2.8V here? Thanks!
Antony
Antony