Part Number: SN74LVC2G74
Hi,
In section 6.3 - Recommended operating conditions, you specify that for Vcc=5V the "Input transition rise or fall time" should be dt/dV=5nS/V (MAX).
Meaning that slow transition might be problematic.
Which inputs does this specification refers to?
I'm asking cause later in the doc, you use an RC circuit on the CLR input presumably to set the output to a known value after the power up.
(At least this is what I intend to do with this input).
But such a circuit will likely violate the transition time spec.
Please elaborate.