Part Number: LSF0204
Other Parts Discussed in Thread: SN74AVC4T774
Hi,
I have some questions about the LSF0204. Basically the LSF0402 is intended to be used as level translator for an SPI communication including all 4 signals (/CS, CLK, MOSI,MISO). I have seen all tutorial videos I came up to some questions.
1- The SPI is shared with other devices such as an EEPROM and digital transceiver (5V) and the level translator is meant for an accelerator (3.3V).
I have placed only one pull up resistor 330ohms in B side for MISO up translation and the rest 3 signals are only meant for down translations.
Would this affect the communication with the other devices ? speed would be limited to the pull up resistor and load capacitance ?
2- The 330ohms is calculated to ensure at least speeds more than 10MHz. In case signal integrity issues, a smaller resistor would help to reach the speed required ?
3- The EN pin as I understood it should be controlled with a push pull output from a uC so no 200Kohms resistor needed for biasing?
Thank you !