This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV594A: SN74LV594APWR Θjc,Pd,Pc

Part Number: SN74LV594A

Hi Team,

Please hep me provide Θjc,Pd,Pc

Part Description
Mfr Name
Mfr Part #
Max Junc.Temp
Θja
Θjc
Pd
Pc
Max Case Temp
Min Op. Temp
PDF SPEC
°C(Tj)
C/W
C/W
(watts)
(watts)
°C(Tc)
°C
 
 
(Ψjt or Θjc)
 
 
 
 
 
 
 
IC,REGISTER,8BIT,S_IN/P_OUT,TSSOP,16P,TR
TEXAS INSTRUMENTS
SN74LV594APWRG4
150
108
?
?
?
N/A
-65
 

-Daisy

  • Hi Daisy,

    Thermal information can be found in section 6.4 Thermal Information of the datasheet. Pd and Pc aren't values I can just give, they are dependent on multiple different variables. I am linking our FAQ page to help you calculate Pd (refer to question 6).

    Pc will need the Icc value and Vcc value. Both of which can be found in the datasheet in section 6.5 (@5.5 V Vcc).