I am using SN74LVC3G34DCUR as a driving buffer to drive 3 leds. The circuit is same as section 9.2 on page 9 of its data sheet to I am debugging the proto now. When I use only channel 1Y to drive a led, the led is very weakly driven, According to my experience with this LED, the driving current is less than 5mA. At the begining, I use 47 ohm current to limit the current. Since it is too weak, I replace 47ohm with 0 ohm to drive led directly. 1A is connected to microcontroller output. I don't know what is could be wrong.