Part Number: TXS0102
Hi,
In my board The TXS0102DCTR is used . the VCCA is connected to 1.8V and the VCCB is connected to 3.3V.
In the TXS0102DCTR Data sheet it's writing that the VCCI is the supply voltage associated with the input port and the Vih is VCCi-0.4.
1. If the I2C signal in port A is 3.3V does it mean that the VCCi = 3.3V?
2.Whether the device can work properly in this situation?
thanks