This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4504B: Is it workable for 3.3V to 5V level shift application

Part Number: CD4504B

Hi Team,

My customer has two applications that to transfer 3.3V signal level to 5V and 15V signal level.

1. I found the datasheet shows that VDD operation range is 5V to 18V, does VCC have same limitation? Is it OK if VCC can operate at 3.3V and input signal level is also 3.3V logic level?

2. If the answer is "no" for Q1, can I power VCC 5V and select pin is at VCC high logic state. Then 3.3V logic level of input signal is acceptable, right? 

Thanks very much.

Vincent