Other Parts Discussed in Thread: SN74LVC32A, CD4072B
Hi,
I have a problem with circuit below. When I plug "O" pins the gate is working without connected VCC. "O" pins comes from camera and they are pulled up to 3.3V inside camera. GND pins are connected together (gate and camera) but VCC pin from gate is not connected to 3.3V from camera. I don't really know why it's working? Is it because of the current flowing by gate input pins? Or inside pull-up resistor (1k) is connecting VCC with 3.3 in some way? If any additional informations are required, please ask me.
Best regards,
Konrad