Part Number: TXB0108
Other Parts Discussed in Thread: SN74LVC245A, SN74LVC244A, SN74LVC16245A
Hi everyone,
I have a question about TXB0108 as voltage buffer. I know TXB0108 is a level shifter and I used it before. Now I want to use it as a voltage buffer but not sure if it can work like that.
Here is the situation:
- A SPI master (like Raspberry PI) needs to drive 12 or more slaves
- CLK speed: 5MHz
- Each slave needs 3 wires (CLK, MOSI and MISO) to be buffered, totally 36 wires (assume 12 slaves). So 5 voltage buffers (TXB0108) are added between master and slaves
- Both sides are working at 3.3V
- The trace is about 20-30cm
Will the method above cause potential problem? Or is it necessary?
Any suggestion is helpful.
Sean