Part Number: LSF0102
Hello,
Regarding to pull down at input on LSF0102, my customer is asking a question.
Their conditions are following.
・Each CMOS buffer is connected to A1 and B1.
CMOS buffer -> A1(input) -> B1(output) -> CMOS buffer
・A1: Pull down (several hundred k ohm)、B1: Pull up (several hundreds k ohm)
(Question)
In this case,
when A1 is low , Is it possible that B1 doesn't go low depending on A1 pull down resistor value?
(Sink current can’t flow enough to pass-transistor from B1 .)
Regards,
Tao2199