Part Number: LSF0102
Hello,
Regarding to input sequence of Vref_A/Vref_B/EN on LSF0102, my customer is asking a question.
(Question)
Do these inputs need to take care the sequence? Or not take care?
Regards,
Tao2199
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Dylan,
Thank for reply.
I have informed your answer to my customer and have additional two questions.
(Question)
・The EN input circuit is designed to be supplied by Vref_B.
When EN and Vref_B are supplied at same time, is there any problem on device?
・Regardless to EN status, before power up (Vref_A or Vref_B) the status of A and B are high impedance.
My understanding is correct?
Regards,
Tao2199
Hi Tao,
From the block diagrams in the datasheet you can see that we recommend connecting the EN pin to Vref B to properly bias the device, so no there are no issues with that. When the supply pins are at 0V, the A and B ports are high impedance. I am linking our Logic Minute videos over the LSF device below. I encourage you to watch them as they will be very helpful in understanding the operation of this device.