Other Parts Discussed in Thread: TXB0104, , LSF0204, SN74LVC2T45, SN74LVC1T45
Would like to connect the interface device having 5V with Raspberry pi SPI (3)
is that possible to use level shifter (SN74LVC245A) or should we use TxB0104 bi-directional level Shitfer ?
Interface device breakout board with 5V communicate with RPI over SPI 4 Wires
-
SCK
-
MISO
-
MOSI
-
SS to
Level Shifter SN74LVC245A is also meant for SPI communication.