Part Number: TXB0304
Hello Team , please help me with below query
We are using this level translator TXB0304 in our design.The application of this level translator is in between FPGA (HP I/O bank voltage-1.2/1.8V ) and QSPI NOR flash at fixed 1.8V. The FPGA side voltage is adjustable and can be 1.2V and 1.8V
Could you please confirm whether we can use this level translator in above application?(Some time both side of the TXB0304 will be at 1.8V)
Also in datasheet its recommended to pull down the OE pin of TXB0304.Is it really required? Can we pull up the OE pin all the time to VCCA side?