This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G08: SN74LVC1G08DCKR pin Y output without Vcc resistivity

Part Number: SN74LVC1G08
Hi Team,
 
I used SN74LVC1G08DCKR on schematic design, I have a question need to clarify.

1.      When VCC is power off, we designed external pull-down to GND resistor on Pin A(1) and Pin B(2).

According to IC design, is there any possible to let pin Y output low? (The VCC is still power off.)

If the answer is true, do you have internal impedance for reference?

SN74LVC1G08DCKR 

  • Hi,

    Could you try and attach the schematic again the current link is broken so I can't see what you are talking about? Just from the description I can say there will be no output state when the device has no supply and the output will be in high impedance.