Hi,
Please tell me the Pd(power dissipation) and θja, θjc (thermal resistance) of SN74BCT25244.
Our customer need this information for thermal design.
According to data sheet P1, 5V * 188mA * 8ch = 7.52W
On the other hand, Abs maximam ratings, any output in the low state = 376mA
So, I think static power disspation is 5V * 376mA * 8ch = 15.04W
This value is so large that I can not judge whether it is correct or not.
Best regards,
Hiroshi