This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SHIFT REGISTER

Guru 13485 points

Other Parts Discussed in Thread: SN74LS673, SN74HC164, SN74HC595

Looking for 8 bit shift register ,same  as the the 16 bit 74LS673 function

  • Hi Eli,
    What do you mean by "same as"? We offer the SN74LS673, which is exactly the same... but if you want something in 8 bit, that's obviously going to be quite different. Are you looking for something in the same (extremely out-dated) technology, or just a standard 8-bit shift register?

    My first recommendation would be the SN74HC164 and the SN74HC595, depending on your use case.
  • I meant same functionality device,but with 8 bit only
    B.Regards
  • I don't know of an 8-bit device with exactly the same feature set as the '673, however the aforementioned SN74HC595 is a very broadly used 8-bit serial-in / parallel-out shift register that has all the features I think are really necessary for such a device. That would be my top choice.

    Additionally, the '595 is available in the X1QFN package that makes it able to squeeze into exceptionally small spaces when needed.