Part Number: SN74LS06
Dear Sir,
My customer met an intermittent (once a year, 24hrs/day) fail that SN74LS06N output stays low when inputing 100kHz 50 to 90% duty square signal.
The circuit is as follows. Three parallel inverters drive OnSemi BD135B family power transistor thru 1kohm pull up resisto to 15Vdc. (changed 500ohm but not solved).
Power off-on toggle reset the fail and work after power on reset.
I am not sure it this is latch-up or this circuit have any potential issue.
May I get your advice if you have some idea to improve this kind of error?
Best regards,
Masa