This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC8T245: Minimum VCC

Part Number: SN74LVC8T245
Other Parts Discussed in Thread: SN74AVC8T245, , SN74AXC8T245

Hello,

I've been having some trouble with the SN74AVC8T245: https://e2e.ti.com/support/interface/voltage_level/f/391/t/697269

I'm planning on migrating to the SN74LVC8T245 and have the same question.    What's the minimum VCCx at which the part will operate?

Don

  • Hi Donald,

    The same answer applies to this device with the exception that the min VCC spec is 1.65 V instead of 1.2 V. I recommend migrating to the new SN74AXC8T245 instead of the SN74LVC8T245 (unless you are trying to translate up to 5 V). This device offers better power on glitch performance, faster data rate, and has a wider VCC range than the SN74AVC8T245.