Other Parts Discussed in Thread: SN74LV4T125
Hello,
I have a small question regarding the workflow of the SN74LVC2G07 part. From the table on page 3 of the datasheet we can see that for 5V VCC the High level Input Voltage should be 0.7 x VCC, i.e. 3.5V. What happens if it is lower? I have 3.3V input voltage, what will I have on the Output? (I assume still high level but a bit lower...?)
I basically want to drive a LED with this part. The LED is connected to 5V and should be controlled with a uC. (see image below)
Kind Regards,
Den