Other Parts Discussed in Thread: TDA2, TDA2E, TXB0104
Hi Team
My customer is now using our TXB0104-Q1. It works from A ports to B ports, but it doesn't work when using B ports to A ports.
B ports are from VP (TDA2) GPIO, and A port goes to DS90UB953 GPIO. The level of B ports are 3.3V, but when connected to B ports, the voltage changes to 0.5V. We tried several things:
1. Disconnect B ports with VP GPIO, the output of VP GPIO is 3.3V. When connected GPIO to B ports, the voltage changes to 0.5V
2. Disconnect A ports with 953 GPIO, which means leaving A ports floating, it's still 0.5V
3. When set 953 GPIO (1.8V) to output, we can get 3.3V output on B ports
4. All ports (A1-3 & B1-3) have the same phenomenon, we changed the chip, it still doesn't work.
5. 3.3V and 1.8V VDD1 power supply is good.
Could you help look into this?
Thanks,
Cera