Part Number: TXS0108E
Other Parts Discussed in Thread: SN74AXC8T245
Dear E2E:
I Download TXS0108E Datsheet , the Operating free-air temperature: –40~125 °C
but i check the temperturen range on TI.COM; I found the operation temperture change to –40~85 °C.
i was a little confused whick value is right. and i want my package is 20BGA MICROSTAR JUNIOR.
By the way: if txs0108e was not suitable, can you help me introduce the right part number.
parameter: 8ch, the max.operation temperture above 105 °C, and the package size below 8 mm2.
thanks a lot.