This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHC123A: What is the threshold level and hysteresis of the Schmitt-Trigger logic inputs?

Part Number: SN74AHC123A


The actual data sheet (October 2005) is talking about: "Schmitt-Trigger circuitry on /A, B and /CLR inputs for slow input transition rates". Later on standard logic input levels for high: VIH ≥ 3.85V @ Vcc = 5.5V and for low: VIL ≤ 1.65V @ Vcc = 5V is given. Do these levels correspond to the threshold level with hysteresis? Thank you in advance for any kind of helpful information.