Other Parts Discussed in Thread: PCA9517, PCA9515A
Hi, experts.
I have two questions about the application of PCA9517 ,
1) The supply voltage of side A ranges of 0.9V to 5.5V , but side B ranges of 2.7V to 5.5V, why is it different ?
Why we cannot design the IC use the same voltage range?
2)There is a description in the datasheet like below, why the B side cannot be used in series ?
"This type of design on the B side prevents it from being used in series with the PCA9515A and another
PCA9517 (B side). This is because these devices do not recognize buffered low signals as a valid low and do
not propagate it as a buffered low again."
Thanks for your attention.
Ready