Other Parts Discussed in Thread: DS16F95QML, SN74AUP1T34, SN74LV1T34, SN74AXC1T45, SN74LVC1G34, SN74AHC1G125
One of our customer connect our board with FPGA chip and TXB0108 on IO lines to the RS485 transceiver DS16F95QML. Are there any potential problems for such connection?
The RS485 is operated in half duplex mode. By default, on power on, 485 is in receive mode. So with the fail safe biasing present (Vab > 0.2) the output of the RS485 IC is expected to be high when no transmitter is driving the differential line. The customer noticed some issues on the IOs.
Bellow the customer's observations:
- the FPGA is powered OFF -> the output of the RS485 IC is going high.
- the FPGA is powered ON with pull up enabled on the IO -> the output of the RS485 IC is going low.