Hi team,
Please help to reply for the one shot related questions as below:
1. Because the TXS0104 can identify the data transmit direction, so for the one shot trigger level is the 1/2 Vin, so for below test signal:
The data direction is from A to B. Signal A is the 1.8V and signal B is 3.3V. So when the input voltage increase up to 500mV, the one shot is triggered. So the slew rate signal B increase. But at the same time, the slew rate of signal A also increase. Does the one shot also affect the input signal?
2.Is there any requirement for the slew rate of the input signal to trigger the one shot?
3.for the below input signal(A), is the one shoot triggered? Does the signal of the output make sense? it seems the output B cannot reach the 3.3V.
A input:1.8V, B output:3.3V
Lacey
Thanks a lot!