Part Number: SN74AUP2G80
Other Parts Discussed in Thread: SN74LVC2G14, SN74LVC1G74
We originally were going to use this IC: www.mouser.ca/.../STM6600DA55DM6F , in order to convert a momentary push button switch to maintain switch.
However, we're using 2 batteries at 1.2V each (2.4V total). The device works with 1.6V (minimum), but it does not enable the output to power up the system if the voltage input is less than 2.5V when button is pressed.
Can you offer a TI product that would achieve the same thing but that's under the 2.4V? We are also looking for something around the same price (or lower) as the other product (roughly $0.50 in 10,000 quantities).
Let me know if TI offers something like this. I just put that TI part number but not sure if that would work.