This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC191: What is the internal impedance or the pull-up / pull-down resistance value?

Part Number: SN74HC191


Hi,Please tell me.

What is the internal impedance or pull-up / pull-down resistance value of the following four pins?

1.QA~QD output pin

2.CLK

3./LOAD

4./CTEN

best regards,

otake

  • Hello otake,

    The internal resistance for the output pins  Qa-Qd can be calculated using the datasheet as follows.

    Using the VOH voltage and IOH current from the electrical characteristics section of the datasheet

    We can calculate a output impedance using R = V/I as (VCC - VOH)/ IOH
    So this gives a impedance of (4.5-3.84)/.004 = 165 Ohms at (4.5Vcc)
    You can recalculate this value based on the Vcc you are using.

    For the input impedance, that can also be calculated from the datasheet using the digital input leakage specification and calculating R=V/I

    This is for the CLK, /LOAD and /CTEN Pins

    R = (6V/1uA)
    R = 6 Meg Ohms

    This is the minimum impedance, it will likely be higher than this and can be recalculated with the typical values for the current shown in the table.

    Thank You,

    Karan

  • Hi Karan,

    Thank you for your answer.

    It is very easy to understand with detailed answers, Thank you.

    otake.