Dear Sirs or Madams,
I know understand as follows;
-When unidirectional signals are outputted from PortA pins, we do NOT have to add external pullup resistors on PortA pins because
the voltage on these pins are driven to VrefA pin's voltage by this IC.
-When unidirectional signals are outputted from PortB pins, we have to add external pullup resistors on PortB pins because
the voltage on these pins can NOT be driven by this IC. The voltage should be driven by external pullup resistors.
Are above my understandings correct?
Best regards,
Shinsuke Tanaka