This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G17: Question about propagation delay spec

Guru 19645 points
Part Number: SN74LVC1G17


If there tpd spec for no datasheet description condition below, please let me know two points spec.

①Waveform about timing for A and Y for "VCC= 1.8 V, INPUT=3.3V, OUTPUT=1.8V、CL=15pF, RL=1MΩ"

 ※Datasheet is only described 2.8ns_min and 9.9ns_max

②Min~max spec and Waveform about timing for A and Y for "VCC= 1.8 V, INPUT=3.3V, OUTPUT=1.8V、CL=15pF, RL=1MΩ"

 ※Datasheet is not described this condition

Best regards,

Satoshi