This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G17: Asking for the SN74LVC1G17DCKR as audio I2S buffer

Part Number: SN74LVC1G17


Hi Team,

Can we use SN74LVC1G17DCKR as I2S MCLK and Micphone clock buffer?

The MCLK frequency is 24.576MHz.

the MEMS MMIC frequency is 3.3MHz.

BR,

SHH