This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G139: find a part like SN74LVC1G139 but with opposite output status.

Part Number: SN74LVC1G139
Other Parts Discussed in Thread: SN74HC04

Dear expert,

As title, I would like to double check with you.

Below is function table for 1G139, but I am looking for "when A,B are both high, Y0 Y1 Y2 Y3 are L L L H".

Did we have suitable part can be used?

Ben

  • Hi Ben,
    I don't know of any other device like the SN74LVC1G139 (2:4 decoder). I would recommend adding a hex inverter (SN74HC04) to invert the outputs.

    Do you know what this device is being used for? Decoders are most commonly used for chip select circuits, and those are typically active low.