Other Parts Discussed in Thread: SN74LV244A
How much input hysteresis does the SN74HC244 have? Is it more or less than the SN74LV244A device?
We have a situation where the HC244 devices are powered by 5V and there are non-monotonic inputs that ring close to the Vcc/2 level - amplitude is ~ 650mVpp and the period of the ring (single ring) - 8 nsec - see attached waveform. Note the input comes form a bus switch so Voh is about 4V.
There is concern that there will be double clocking in this legacy system and we'd like to know if the LV244A would perform better than the HC244 in this regard - esp considering the hysteresis levels & timing.