Other Parts Discussed in Thread: SN74LVC125A, SN74LV126A, SN74LVC126A, SN74LV125A, SN74AVC8T245, SN74LVC8T245, SN74AVC4T774
Hello!
I wanted to ask if there exists a logic device that has xbits (as much as possible) to act as a logic buffer which I can program the direction via binary code or serial interface?
Basically the idea would be to have a device with 16 bits and 4 address bits which tell the device if bitx is an output buffer or an input buffer (driving about 10mA - 24mA). This device would have the advantage that i can create a default main host controller board where I buffer all available GPIOs and later decide - depending on the actual application - which ports I want to define as an input or output but with the advantage to have all the ports buffered allready.
All available transceivers I have found only have the possibility to change the input/output behaviour for all the bits of one element at a time.
I would be really happy if there exists a device like i've wished for.
best regards
Benjamin