Other Parts Discussed in Thread: TXS02612, , TWL1200
I have an application where I need the SDIO output signals to all be floating or with weak pull-ups when the input is the same. At first I wanted to use TXS02612 along with the SEL pin, but it seems that the CLK signal will be pulled low when not selected. Was wondering if TWL1200-Q1 would work.