Other Parts Discussed in Thread: SN74LV1T125
Hello E2E,
I am posting on behalf of a customer.
We are operating with Vcc at 2.9v We would like to pull OE up to 1.8V which is close to the MIN. Do you have any data on how much buffer there is below the MIN? I did a test in the lab and found the threshold at 1.3V but I am not sure what the part to part variation would be.
Now, I understand that we can't guarantee operation outside of spec of the datasheet, but table 6.3 conveniently doesn't take data at 2.9V... If we assume worst case (Vcc = 3.0V), then they won't eclipse the necessary OE threshold. But if Vcc = 2.7V, then they will pass our datasheet spec. So, do we have data at 2.9V? Will their above conditions work?
Finally, I did warn them about the following from the DS:
To assure the high-impedance state during power up or power down, OE must be tied to VCC through a pullup resistor; the minimum value of the resistor is determined by the current-sinking capability of the driver.
Thanks for the help!
Russell