My customer is using the SN74LVC1G123DCUR to provide a high level output as long as the input is above a certain frequency. Figure 7 of the datasheet gives the minimum retrigger time, which would indicate the minimum frequency required for a given Cext (and supply voltage) to provide this function - but I don't see a mention of Rext in this curve (which would also have an effect on this). What is the Rext value for this curve?
In my customer's testing with an Rext=10k and Cext=0.01uF (supply=3.3V) they see a constant output when the input frequency is >10kHz...
Thanks,
Dan