Hi Team,
My customer use the TXS0104 to translate the voltage for the I2C signal. And they found there is a glitch in rising edge of the SDA signal tested in the B port.(show as below).
Below is the schematic:
1. I have asked them to remove the 2.2K and 4.7K pull up resister, but it seems no help.(see below)
2. In the B port, they also connect the 100pf cap to ground in the SDA and SCL, after they disconnect the 100pf resister, the issue seems to be fixed.
1. Does the 100pf cap cause the issue? If not, what may be the cause?
2. If the 100pf cap can cause the issue, do you have some recommend method to optimal the B port signal?
Lacey
Thanks a lot!