Part Number: SN74AUC2G34
I need a clock buffer that will provide switchable 1.2V or 1.8V CMOS output swing. I propose to use the 74AUC2G34 with switchable supply to select the output level. Source clock is 1.8V CMOS and as I understand 2G34 inputs are over voltage tolerant at this level. However, this part is not characterized as a clock buffer but I would like to know the period and phase jitter. Any possibility that this information is available?