This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G125-Q1: What is the recommend output current at Vcc=3.3?

Part Number: SN74LVC1G125-Q1


Hello

What is the recommend output current at Vcc=3.3? 

The SN74LVC1G125-Q1 . SGES002C–APRIL 2003–REVISED APRIL 2008 datasheet (pg3)  shows 16ma and 24ma for Vcc=3v. 

The datasheet  front page states "±24-mA Output Drive at 3.3 V". 

To max reliability/thermals/life no doubt the lower current drive is better target. However whatis the impact of running at 20ma or 24ma ? 

Seems as if 20ma would be comfortable? 

Thanks & Regards