Part Number: TXS0108E
Dear SIR:
(1)May I have some question regarding the part application TXS0108E ?
As datasheet mention as below:
1.2 V to 3.6 V on A Port and 1.65 V to 5.5 V on B Port (VCCA ≤ VCCB)
We want to know ,That "port" meaning "include pin A1 ,A2, A3, A4, A5, A6, A7,A8 ,B1 ,B2, B3, B4, B5, B6, B7,B8 )?
(2)
If VCCA pin is 1.8V ,VCCB pin is 3.3V
Pin A1 ,A2, A3, A4, A5, A6, A7 ,A8 signal is 1.8V
Pin B1 ,B2, B3, B4, B5, B6, B7,B8 signal is 3.3V
change to below condition : TXS0108E will Work Normally or not ? (nr any advice ?)
VCCA pin is 1.8V ,VCCB pin is 3.3V
Pin A1 ,A2, A3, A4, A5, A6, A7 ,A8 signal is 3.3V
Pin B1 ,B2, B3, B4, B5, B6, B7,B8 signal is 3.3V
Thanks